FB#.RESREFPHASE
Description
This parameter sets the electrical degrees of phase lag in the resolver.
See the motor resolver datasheet for the value for this parameter.
Context
See Feedback Devices.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
electrical degrees |
Range |
-180 to 180° |
Default Value |
-2° |
Data Type |
Float |
See Also |
N/A |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
FB1.RESREFPHASE | 0x3500 | 0x5 | UDINT | - | - | RW | False |
FB2.RESREFPHASE | 0x3501 | 0x5 | UDINT | - | - | RW | False | |
FB3.RESREFPHASE | 0x3502 | 0x5 | UDINT | - | - | RW | False | |
FB4.RESREFPHASE | 0x3503 | 0x5 | UDINT | - | - | RW | False | |
FB5.RESREFPHASE | 0x3504 | 0x5 | UDINT | - | - | RW | False |